Part Number: LMH6654
I'm working on a wide bandwidth signal amplifier. I want to use the LMH6654MF/NOPB as the final output stage. The last amplifier I used had an issue where it worked normally with a 50 ohm DC load, but when the output was AC coupled, it had severe zero-crossing issues as shown below. Will this chip behave normally when AC coupled, or does it still need the 50 ohm DC load?

TLDR: This should work fine. v

But will adding this capacitor break things? v