Part Number: OPA991-Q1
Other Parts Discussed in Thread: OPA991
Hello ,
I have build an high side differential amplifier using OPA991.
In this schematic i have used an offset about 2.5V.
My expectation was that if the current is 12A (1 Ohm load at 12V)the voltage at output of the opamp (pin 1 ) the voltage should be 12mV x 14(amplif|) + 2.5V = 2.668V
Instead of this I have measured a voltage of 2.660V.
Resistors are smd resistors that have 1% tolerance.
Could be this the cause of difference in measurement ?
Thank you