Part Number: TIPD181
Thank you for the circuit design.
However, Would it be possible to provide a design with somewhat larger components?
This one uses 603, which is pretty small.
If you look at the overall PCB size and complexity, there is no logical reason for using 603 size.
It would make building it MUCH easier if a larger size was used: say 805 or larger.
The current PCB is about 90% empty space: it could have used thru hole components actually.
Since the whole idea of this exercise is to show-case the OPA, you would be MUCH better off with a design that's easier to build, especially for those of us who aren't as young as we once were....
If i decide to make a large number, then I can use a small SMC size.
But for a protype it seems silly to use 603.
Thanks,
Alan