Part Number: ISO124
Other Parts Discussed in Thread: ISO224
Hi,
I am going to design a circuit to isolate the ground between 2 sides. So, i planned to go with ISO124. I have some queries related to it.
Input Voltage range : 0V to 10V
Power supply: there +12V supply available , using that isolated +12V can be generated.
Can i connect GND1 and -VS1 together(connect to +12V GND), since my power supply is only +12V.
Similarly at output side also can i connect GND2 and -VS2 together and connect to Isolated +12V GND?
Regards,
Kannan