This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2274AM-MIL: ESD rating

Part Number: TLC2274AM-MIL

What is the ESD rating of TLC2274AMJB?

  • Hey Joey,

    We do not have data on the ESD rating for the TLC2274AMJB. It is likely this data was not collected, as it was not required for release.

    The commercial version of this device has an ESD rating of 2kV HBM and 1kV CDM. However, many factors influence the ESD rating, like package type. This information is given as an example of a similar die design that may have a similar rating but this is not the same as an ESD rating for the TLC2274AMJB.

    Best,
    Jerry