Part Number: LMH32404
Other Parts Discussed in Thread: LMH32401, THS4541, OPA855
Hello,
1. I've noticed that the Pspice model of LMH32404 doesn't seem to support VOD. Regardless of the voltage value connected to this pin in simulations, the output waveform remains unchanged. Have you observed the same behavior?
2. I'm planning to use LMH32404 with a connected photodiode sourcing current into the LMH32404 input. Would the linear range of the device be the same as when the current is being sunk? Spice simulations indicate that the output range is significantly higher when the input current is being sunk compared to when it is sourced.
3. As mentioned earlier, I intend to use the LMH32404 with the photodiode sourcing the current. In this mode, I would need to apply a negative value for the VOD input. This is to ensure that under no light conditions (of the photodiode, the differential output is not zero but rather negative. This is necessary for interfacing with an ADC that utilizes 2's complement for its data output. Can the VOD input accept negative values?
Thank you,
Sariel
Hi Nick,