Part Number: OPA855
Other Parts Discussed in Thread: LMH6624, OPA859
Hi,
The Great thank for suggesting OPA855.
Trailing from
I used OPA855 on same board with all correction from above conversation.
PCB assembled as per EVM circuit --> OPA855IDSGEVM , app note--> sbou210, all values matches with EVM circuits recommended values.
R6 = 0E, R7 = Not assembled (It was giving zero output), First OPAM output connected directly to second, and so on. All other components used as it is.
No oscillation at output of any OPAM observed as seen previous with IC LMH6624. (I think this OPA855 working fine) and taken below readings.
3 OPAM working fine in series.
Input voltage is 20mV AC 25MHz.
IC VCC = 2.2V, VEE = -2.2V. Input signal is taken from
When assembled fourth OPAM --> output is not acceptable.
OPAM 1 OUTPUT.

OPAM 2 OUTPUT.

OPAM 3 OUTPUT.

OPAM 4 OUTPUT.

Q1- what can be reason that OPAM 4 is saturated? Even when input voltage 1mV AC 25MHz. (Input voltage is given form function generator. Function generator output voltage is nearly accurate.)
Q2- why AC signal shifting by adding some voltage?
Q3- why gain calculation of EVM, not matching with results. Even I checked EVM, for one OPAM output, result is same.