Part Number: LM2903B-Q1
Hi expert,
Hope you are doing well.
For LM2903B-Q1, when VCC is 0, IN+ is in 0-20mV, IN- is 0, the output is in open-drain form, why output would be pulled down? (detected as low)

Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2903B-Q1
Hi expert,
Hope you are doing well.
For LM2903B-Q1, when VCC is 0, IN+ is in 0-20mV, IN- is 0, the output is in open-drain form, why output would be pulled down? (detected as low)

Thanks.
Hello Daniel,
If VCC is 0V, there is no voltage available to turn on the output transistor (Vbe > 0.55V). The output starts to function when VCC > 1.3V, but that is still not enough voltage to bias the input stage - so the input stage is still dead. Even if there was some path from the input to the output, 20mV is not enough to turn on the transistor.
Are you seeing some devices pulling low? Does it work normally when powered?
I have not ever seen the output pull low with no supply unless it was damaged.