This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1301: AMC1301 OUTPUT have 0.6V issue

Part Number: AMC1301


Hi, Support Team

We have a question if  VRb=0V, and we find output offset have 0.6v?  is normal?

schematic:

if any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence

  • Hi Lawrence,

    No, this would not be considered normal as the input offset voltage is specified to be 0.2mV (max) input referred or 1.64mV referred to the output. 

    Do you mean "V_A" = 0V when you say VRb = 0V?

    Is the R3' resistor, R56 installed? 

    What are the outputs connected to off picture in the schematic?