Other Parts Discussed in Thread: OPA814,
Hi TI team,
I noticed something strange when it checked the Datasheet.
OPA656UB/2K5 is a Hi-Grede model of OPA656U/2K5, but the spec below seems like OPA656UB/2K5 is Down-Spec.
Max. Input Bias Current(pA) for VCM=0V, TJ=25℃
OPA656U/2K5: +-20pA
OPA656UB/2K5: +-450pA
Is +-450pA the correct value?
I also noticed that there are two Input Bias Currents with the same content. Is this Typo?
Also, in Section 7.6, are CMRR and PSRR OK to compare with Electrical Characteristics (continued)? There was no (continued) in the item 7.6.
Thanks and Best Regards,
Akira Ono