Hi expert,
My customer find some issue about Ref pin floating or give it a 3.5kohm will see the output signal have 10khz abnormal noise as this pic
their original circuit connect is Ref pin and Gnd pin connect together then connect to RTN (system Gnd), but REF pin and Gnd pin open (did not connect RTN) will see output like pic.
so they have two question as bleow
Q1.why output will see like this ?
Q2.output pin has this noise cause from REF pin or Gnd pin or both will impact ?


Then they try to use the auto resistor connect between GND/REF to RTN before power up and they give 3 section by different resistor value.
blue one is 3.5kohm
green one is <1ohm
orange one is 10kohm
and they have 2 question about this result
Q3. Why section 3(orange) is also high impedance and output result can not see like section1(Blue)
Q4.Before power up GND/REF pin to RTN status will impact output pin performance and why the root cause ? (because section 3 also high impedance but not any risk on output)

Please help on comment these 4quesion. THanks!
Eddie