Part Number: OPA657
Other Parts Discussed in Thread: OPA818
Hi, I'm using the OPA657 as transimpedance amplifier(TIA), and also reading datasheet of OPA657.
I find it states 'OPA657 has 1.6GHz Gain-Bandwidth Product(GBWP)' and also figures open loop gain graph (magnitude and phase).
I think there are two poles in graph (between 100Hz and 1GHz), maybe 500kHz and 200MHz or 300MHz.
Anyway I have question about GBWP. This graph has intercept at 800MHz (when magnitude=0dB).
This specification doesn't match with 1.6GHz GBWP.
How can I interpret this?
Thanks.