Hi!
I bought an INA826EVM. I needed to change the INA chip itself. But I also needed to attach a potentiometer as Rg (gain regulator resistor). But the soldering points are about or less than 1 mm2, and they are situated about or less than 1 mm apart. I think those are very narrow margins - unnecessarily small. It would be more practical with larger soldering points and a larger distance between them. Thank you. :-)