Part Number: INA211
Hi Team,
How to calculate what is the minimum current that can be measured using the INA21x Solution ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA211
Hi Team,
How to calculate what is the minimum current that can be measured using the INA21x Solution ?
Hi Clemens,
Thanks for the input.
Have one more Query, in data sheet they have given like "Enables Shunt Drops of 10-mV Full-Scale".
What does it mean? Whether the shunt drop should be minimum 10mV to get the better readings? Below image shows the data.

Typical shunt resistors are larger, with something like 100 mV at full scale. The low offset voltage of the INA211 allows smaller shunt resistors.
With a full-scale voltage of 10000 µV, the 35 µV offset would result in an error of 0.35 %.
The datasheet specifies no minimum. You have to decide yourself what error you can accept.
Hi Chandrashekhar,
Thanks for the question and using the E2E forum.
Along with the responses from Clemens (thanks Clemens!), here's a video we've put together that should help in picking an appropriate shunt resistor for your application.
Please let us know if you have any other questions.
Louis