ABS max is +/- 6.5V, but I assume it's just the delta of 13V? e.g Can 3.3 to -8.0V also be used because the delta voltage is under 13V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ABS max is +/- 6.5V, but I assume it's just the delta of 13V? e.g Can 3.3 to -8.0V also be used because the delta voltage is under 13V?
This device does not have a ground pin and so does not know what voltage you choose as 0 V. The maximum indeed is 13 V between the two supply pins.
(If your signals are around 0 V, and if your supplies are very asymmetric, you have to consider the valid common-mode input voltage range.)