Other Parts Discussed in Thread: INA232
INA231 was claimed that it is a bidirectional part. Can it support bidirectional current at low side?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
"Bidirectional" means that it can measure current flowing in the opposite direction, i.e., IN+ having a lower voltage than IN−. This is supported for both high-side and low-side configurations, over the entire common-mode voltage range.
Thanks Clemens!
Yuan,
Let me know if you have any further questions.
Regards,
Mitch
Yes, that would be outside the common-mode voltage range.
You could connect the INA231's GND to a lower voltage. Or use some other device (e.g., INA232) that can go down to −0.3 V (if this is enough). Or combine a difference amplifier with an ADC.