This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9302: Rating for the input signal

Part Number: TLV9302


Hi team,

The maximum rating of the signal input pins is specified with respect to the supply voltage.
What happens if the input voltage is applied without power supply?

I understood that there is a clamping diode that is capable up to  +/-10mA. So, if there is a limiting resistor the input current is guaranteed to be less than 10mA, can the customer exceed (V+) + 0.5?

Regards,

Ohashi