Other Parts Discussed in Thread: TL074
Hi team
They think to use TL074HIDR instead of TL074CNSR becuase TL074CNSR will be EOL. So they want to know the difference.
1. Regarding electrical characteristics, they want to compare these devices at Vs = +/-15V. In the datasheet, TL074CNSR is defined at VS = (VCC+) – (VCC–) = ±15 V while TL074HIDR is defined at VS = (VCC+) – (VCC–) = 4.5 V to 40 V (±2.25 V to ±20 V). Does this mean it is OK to use the characteristics of TL074HIDR in order to compare these devices at Vs = +/-15V?
2. Are there any comparison tables of these devices?
Regards,
Noriyuki Takahashi