Part Number: LM2903
Other Parts Discussed in Thread: LM393LV, TLV7211, LM339, , TLV1851, LM4040-N, TLV6703, TL331B
Hi,
I hope you are doing well. I would like to use Texas Instruments LM2903 IC for the purpose of monitoring the voltage level of my intrinsically safe battery assembly by performing a voltage comparison of the power supply voltage to the comparator voltage which will be set by a Zener Diode with a nominal voltage of 8.2 V.
Given that the nature of my application of instrinsic safety I need to limit the power that can faulted to the IC. One of the pathways is through the VCC connection. Therefore, I'd like to add a resistor to the track feeding the VCC connection. My battery assembly will have three 3.6 V cells in series resulting in a combined voltage of 10.8 V. Based on the datasheet family comparison table the IC consumes a maximum of 2.5 mA. Assuming a 1000 ohm resistor is installed on the VCC track this will result in a voltage drop of 2.5 V (2.5 mA x 1000 ohms = 2.5 V) and therefore 8.3 V will be supplied to the IC under this scenario (10.8 V - 2.5 V = 8.3 V) which is above the minimum supply voltage of (-0.3 V) according to section 6.1 Absolute Maximum Ratings Table.
Can you please advise regarding whether this conclusion is accurate and I can proceed with installing the 1000 ohm resistor on the track feeding the VCC connection on your LM2903 IC.
Thanks in advance for your support.
Best regards,
Joe DeWitt