Part Number: THS4551
Other Parts Discussed in Thread: LMH34400
In the datasheet in section 8.7 (Terminology and Application Assumptions) it states:
"Good power-supply decoupling is required. Often a larger capacitor (2.2 µF, typical) is used along with a high-frequency, 0.1-µF supply decoupling capacitor at the device supply pins (share this capacitor with the four supply pins in the RGT package). For single-supply operation, only the positive supply has these capacitors. Where a split supply is used, connect these capacitors to ground on both sides with the larger capacitor placed some distance from the package and shared among multiple channels of the THS4551, if used. A separate 0.1-µF capacitor must be provided to each device at the device power pins. With cascaded or multiple parallel channels, including ferrite beads from the larger capacitor to the local high-frequency decoupling capacitor is often useful."
The above is not useful and the author appears to be ignorant of capacitor technology that's been commonly available years before the datasheet (dated 2022). A 2.2uF X7R in an 0603 package _is_ a good high frequency decoupling capacitor. Paralleling it with an 0.1uF X7R capacitor would create a huge spike in impedance, caused by the parasitic L of the 2.2uF resonates with the C of the 0.1uF. To damp this down a resistor in series with the 2.2uF could be used or a capacitor with an inherently higher ESR than X7R caps, such as a tantalum or aluminium electrolytic. The last sentence stating that ferrite beads are often "useful" does not explain what problem with the THS4551 they solve or which ferrite bead(s) to use. I would guess is it coupling from one amplifier to another through the supply rails, which is much more predictably dealt with by using series resistors of a few ohms rather than ferrite beads.
Here is what I think is a more rational and useful way to determine the amount of decoupling required for the amplifier:
1) If the bandwidth of the input signal is BW Hz then, to a first order approximation, the variation in the supply current of the amplifier will also have a bandwidth of BW Hz.
2) For a signal superimposed on the supply then the amount of that signal at the output of the amplifier is equal to the PSRR of the amplifier at the frequency of the superimposed signal multiplied by the gain of the amplifier.
3) The amplitude of the variation of the supply current is equal to the output voltage swing divided by the load resistance, with the (unachievable) worst case for a RRO amplifier being the supply voltage divided by the load resistance.
Let's put some number in and see what comes out.
Vcc = 3V; Vee = 0V; Rload = 100-ohm; BW = DC to 20MHz; Gain = 0dB
The PSRR+ for the THS4551 is falling at -6dB/octave from ~85dB @ 5MHz, so at 20MHz the PSRR would be ~73dB. With gain = 0dB, the gain from Vcc to the output is (0 - 65) = -73dB
The maximum variation in supply current Vcc / Rload = 3V / 100-ohm = 30mA.
With a single 2.2uF X7R 0603 used for decoupling for each THS4551:
Impedance at 20MHz is limited by the capacitor + mounting inductance. Assuming a total of 2nH the impedance is ~0.25-ohm. With the 30mA supply variation this would induce a ripple voltage on the supply of 7.5mV. At the output this would introduce a ripple of ~1.7uVpp in a 6Vpp output, or -131dB lower than the output signal.
At 10kHz the impedance of the 2.2uF is ~7-ohms, so the ripple voltage would increase to 210mV. However, at 10kHz the PSRR improves to 105dB. At the output this would introduce a ripple of ~1.2uVpp in a 6Vpp output, or -134dB lower than the output signal. In reality at 10kHz and lower frequencies other "bulk" capacitors on the board and the output impedance of the voltage regulator would push the impedance well below 7-ohms, leading to even lower voltage ripple.
If isolation between amplifiers is needed then using, for example, a 2.2-ohm resistor in the power supply to each amplifier would form an RC low pass filter with the 2.2uF decoupling capacitor for each THS4551 with a -3dB frequency of ~33kHz. The peak to peak output swing, even into 100-ohm load, would be reduced by less than 150mV. Using a resistor avoids LC resonance that can be caused by using ferrite beads and the effect of changing values is predictable.
In summary:
Ignore the datasheet's advice on decoupling and do your own analysis. If you can't be bothered to do an analysis then a 2.2uF 0603 X7R per THS4551, possibly with a series resistor of a few ohms if isolation between amplifiers is required, should be good enough for the following applications:
- Gain close to 1 driving a heavy load (100-ohm) with large output swing. E.g., ADC driver.
- Gain much larger than 1 driving a light load (> 1k-ohm) with large output swing or a heavy load with small output swing.
Hopefully this will be of help to someone and might inspire the engineers who produce the datasheets at TI to up their game and not just paste boilerplate "advice" for decoupling circa. 1990 ;-)