Other Parts Discussed in Thread: TPA3255
Hello,
I've encountered some challenges in designing a product that involves using a TPA3255EVM evaluation board. Initially, the evaluation board performed well in powering a small three-phase motor, meeting the product requirements effectively.
However, when I designed my PCB based on the TPA3255EVM schematic and sourced the chip from Mouser (refer to the link), the performance fell short. The new PCB doesn't deliver as much power as the development board, despite generating a similar voltage waveform. It appears unable to provide sufficient current to drive the motor under load conditions. When increasing the voltage to start the motor, it runs at lower voltages, but under even a slight load, the waveform disappears, resulting in a flat line. Additionally, the motor struggles to initiate movement at higher voltages.
Comparing this to the development board, I never encountered these issues. I am uncertain if the chip on my board is identical to the one on the development board.
Could you help me understand if the chip I am using matches the one employed in the development board? I have also linked the schematic of the amplifier part of PCB.
https://www.mouser.co.uk/ProductDetail/Texas-Instruments/TPA3255DDVR?qs=KuuZdrM3jLz8froI3AXsFA%3D%3D
Thanks,