Part Number: TL081
Other Parts Discussed in Thread: TL061, TL031, TLE2021
Hello
PDIP(8) is used as a replacement for obsolete products.
Initially, we considered TL081IP. but
Regarding the Temperature coefficient of input offset, we calculated it from the answer below and found it to be 150uV/℃@(25-85)℃(MAX), which is too large.
>TL081 is 18uV/C typical, maximum wouldn't create 15mV of Vos;
I would like to adopt the TLP031IP, but please let me know the following as soon as possible.
(1) Use by attaching a 10kΩ trimmer resistor between the offset and NULL terminals and connecting the tap to -12V. at this time
ΔVIO(adj)(Offset voltage adjust range)
Does it satisfy ±15mV (TYP)?
(2) In the Input Offset-Voltage Null Circuit of TL061, a 1.5kΩ center resistor is attached to the 100kΩ trimmer resistor.
Are there any major problems when using the TLP031IP with a 10kΩ trimmer resistor and connecting the center tap directly to -12V?
(3) TLP031IP has JFET input, is there anything I should be careful about when using it?
For example, phase, gain margin, open loop gain, minimum gain, ringing due to feedback circuit response delay, etc.
Best regards