Part Number: LM324
Hey,


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM324
Hey,


This voltage is inside the absolute maximum ratings, so the device will not be damaged.
This voltage is outside the valid common-mode voltage range, so the behaviour of the output is not guaranteed. (In practice, it will try to go towards the positive rail; see section 2.2 of the Application Design Guidelines for LM324 and LM358 Devices.)
Hey Clemens,
Please refer to the queries mentioned below-
1. You're talking about the absolute maximum ratings- 30V, right? IC won't get damaged if input is within this range?
2. It means even if we provide 3.3V power supply at VCC, the output may increase from 3.3V to 5.5V (if we are providing 5.5V at the input of the opamp)??
1. Correct.
2. No, the output will try to go towards 3.3 V, but will not reach it (see the VOH specification).
Hello Shivangi,
The output range of LM324 is about 0V to 1.8V at 25C and less range at -40C. If sinking much output current then things get worse.
The output range of LM324A is better, 0V to 3.3V
For both, the valid input common mode range doesn't go up to 3.3V
Why was 5.5V chosen for EXT_ADC1?