Part Number: BUF802
Customer is using BUF802 in the standalone configuration. Their application does not need the DC performance on the BUF802 that the composite loop provides, so the standalone configuration will make their design much simpler.
It was noted that the input offset voltage is nominally -600mV from the datasheet, which is observed in simulation.
1. Does this degrade the output swing of the BUF802?
2. Is there a way to minimize or remove it, or is the only option to AC couple the output?