Part Number: OPA1S2384EVM
Other Parts Discussed in Thread: OPA1S2384
Hi Jonard,
I am going to test TIA circuit using OPA1S2384.
Negative input(-IN A) is used for PD input adding R6 (0R), input(+In A) is ground.
Input signal from signal generator is 50mVpp.
1st stage OutA is working with inverted output.
But Even I try to invert signal, when I checked 2nd stage Out B, is working with buffer mode.
In order to invert 2nd OpAmp, below configuration is used.
- SC is open (Low).
- TP1 and TP7 is tied.
- But when I check connectivity between Pin2(IN S) and Pin6(+IN B), it looks tied with 6Ohm. That is why Out B is not inverted.
Please review my configuration, I am looking forward seeing your reply ASAP.
Thanks