Part Number: OPA567
Other Parts Discussed in Thread: INA317
Hi,TI expert
I have a TEC application question when I use opa567. My schematic is shown in the pic below.
Vset is the voltage corresponding to the set temperature,Vth is the voltage fed back by the thermistor. I replace ad623 in the pic with ina317. R11 is replaced by a laser in real schematics. If Vset=Vth, then VTEC+=VTEC- theoretically.
But in real experiments, I set Vset=1V, coresponding 25℃, and the feedback voltage Vth is smaller than 1V,about 0.9V——translateing to 28° in laser. The temperature is stable at 28°. VTEC+=VTEC-.
Why can laser temperature be stable when Vset and Vth are not equal.
Thanks