Other Parts Discussed in Thread: LMH6642, TLV365
Original | New (Alternate) |
LMH6643MA/NOPB
|
XTLV2365
|
LMH6642MF/NOPB
|
TLV365DBV
|
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original | New (Alternate) |
LMH6643MA/NOPB
|
XTLV2365
|
LMH6642MF/NOPB
|
TLV365DBV
|
Hello Praneeta,
I can work to assist with this project. Could you confirm your gain settings for both amplifier stages, as well as the characteristics of your input signals, output loading, and power supply (VIRIS)?
The gain-bandwidth product of the TLV365 (50 MHz) is lower than the LMH6642 (57MHz), but both parts are voltage-feedback op-amps and should operate similarly to each other.
Could you explain more about the IRIS motor only working in one direction?
Best,
Alec
Hi Alec,
Sorry for the delayed response,
I will just give a brief for this circuit and the testing we have done till now,
Through this circuit, we are trying to run the DC motor and that will work in one direction only U16 IC is just working as a buffer and there is no issue due to U16 we have checked that, the U5 IC is working as an op-amp voltage comparator and we are facing the issue due to this IC only, this may be due to reason TLV365DBV operating time is more than LMH6642MF/NOPB so it is not able to respond as per our existing setting. power supply (VIRIS) is 3.3V.
Today we have done one iteration and were able to find one solution, we tried placing 0.1uF on the R55 Resistor Pad as shown in the attached image and Now IRIS is working properly the same as the OLD design.
Can you please see and tell us what exact parameter of Op-amp is causing the issue?
Hello Praneeta,
This is a very interesting fix to the circuit. The major difference between these devices is the bandwidth and slew rate of the devices as most of the other specs are similar. Is there any information you can give as to why this capacitor was placed in this location or if there were other spots that also worked when adjusting the circuit?
Best Regards,
Ignacio