This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2192: OPA2192 internal diodes and ESD detail

Part Number: OPA2192
Other Parts Discussed in Thread: OPA192

Hi Expert,

My customer use OPA2192 on their board as pic.

and they find one wire issue and his setting as bleow;

No Vcc , Pin3 no input signal , take out the resistor as the blue X.

only 4V from VLSI , but they see OPA192 PIN5 only 2.4V on there.

So 1.6V just gone , they suspect the IC internal has some diode or ESD way pass trough then take out the VLSI voltage from PIN5.

Do you have any comment  ? because no vcc and one channel also no signal .

why input voltage will not see the same between input side(VLSI 4V) and pin5 ?    

Eddie