Part Number: VCA821
Other Parts Discussed in Thread: TINA-TI
Hello I want to use VCA821 to design the input DC signal range in 0-1v or 0-2v Through the DAC input control chip pin Vg to achieve the output range of 0-3.3V, VCA chip power supply ± 5v Look at the data sheet, showing the input range ±Vs, but I downloaded the Tina simulation model on the official website SBOM366.TSC for simulation testing, but modified the Rf to 402Ω Rg to 18Ω The test operation is as follows: (1) The fixed Vg is 0.45V Input 1V output is 67.17mv, input 100mv output is 47mv (2) fixed Vg is 1V input 0.1V, output is 1.72V, input 0.2V, output 1.84, Vout/Vin ratio amplification is inconsistent, I don't know what the reason is.
I don't know if you can help modify the peripheral configuration circuit in the case of the simulation model on the official website, so as to realize the input DC range of VCA821 0-1v or 0-2v, and adjust the Vg to make its output range 0-3.3V