Part Number: LM2901
Other Parts Discussed in Thread: LM339LV,
Hi,
The customer finds a problem. When LM2901DR is supplied with 3.3V power, the output fails under -10 ° C in a low temperature environment. The waveform is as below, and the output failed, cannot be stabilized. The temperature range indicated in the datasheet is -40~125; In 5V power supply does not have this problem, high temperature test also passed. To do ABA verification, the bad chip was changed to a 5V powered circuit board and the low temperature test was normal.
May I ask what causes this?
-40℃ output
-20℃
-4℃