Part Number: OPA188
Other Parts Discussed in Thread: OPA171, OPA277, OPA196, OPA197, OPA191, OPA192
Hi all,
My customer is trying to realize a circuit that uses OPA188 to full-wave rectify an AC waveform, integrates it in the subsequent amplifier, and outputs DC proportional to the input amplitude.
When inputting a signal of Vpp = 300mV and 20kHz to a rectifier circuit, an oscillation-like waveform is observed.
Why does this oscillating waveform occur?
The red waveform is the input waveform.
The blue waveform is the offset voltage waveform.
Yellow is the output of OPA188.
Green is the waveform after rectification.
In addition, such oscillation waveforms were not observed with OPA277 and OPA171.
I would like to send the circuit diagram via private email later.

Regards,
Toshi