Part Number: INA228
Other Parts Discussed in Thread: ISO1640, ISO1641, , INA233, BQ76942
Hello,
I'm working on a circuit based on STM mCU, with some I2C devices used. One INA233 and one INA228 device is placed on mCU's I2C side, wheras BQ76942 is used remotely. Its I2C lines are isolated from mCU's I2C lines with ISO1640 isolator. ISO1640 isolator is used instead of ISO1641, because ISO1640 supports also devices that perform clock stretching and BQ76942 performs clock stretching.
A problem is that Vol1 of ISO1640 is 570 mV (min.) and 710 mV (max.) which is higher than VIL(max.) of both - INA233 and INA228 that equals 0.4 V.
Since INA233 and INA228 would just listening what BQ76942 will replying (via ISO1640) to the mCU, could this lead to glitchy behaviour of INA233 and INA228 devices? mCU on the other side have VIL (max.) higher than Vol1 of ISO1640, so there will be no a problem with mCU.
Below is a schematic:

I must say that I already have some circuits which are simmilar - there are also INA233 used, but ISO1641 is used instead of ISO1640. However ISO1641's SDA line has also very high VOL on the side 1, which is higher than VIL of INA233, but it looks like that everything works without problems.
Can you please confirm that because INA233 and INA228 will just "listening" what BQ76942 IC will replying to mCU via ISO1640, this would not lead to glitchy behaviour of INA233 and INA228?
Many thanks,
Kind regards,
Dejan.