Part Number: PGA309
Hello,
One customer meets the bandwidth question about PGA309.
1) .The signal generator output sinewave with +-20mV, adding 2.5V bias to PGA309 input to meet the input common voltage requirement.
2) The front PGA Gain=32, Gain DAC=0.5, output amplifier GAIN=2.
2) Changing the frequency of sinewave, from 20Hz~200Hz, record the frequency and output amplitude.
He found that the bandwidth is 165Hz, while the datasheet described that the front-PGA bandwidth is 60Khz ,and the output amplifier bandwidth is 2Mhz.
Because there is no PGA309 spice model for simulation, so I need your advice.
Thank you very much for your help.
Best regards
Kailyn