Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA281-Q1: INA281-Q1 related issues

Part Number: INA281-Q1

HI,

Can the VS pin of INA281-Q1 be connected to Vcm, and can the power supply voltage and detection voltage be connected together, as shown in the following figure:

  • Hello Valued Engineer,

    Yes. The device can be powered up off the same bus the input pins are connected to as long as the Vs pin does not exceed 20V (to maintain specified performance) nor 22V (to not exceed Absolute Maximum rating and become damaged).

    The devices specifications are tested for Vs up to 20V so accuracy and performance may degrade for Vs >20V, but < 22V. The device itself is rated to survive Vs voltages up to 22V according to the Absolute Maximum Ratings table.

    Another thing to consider is that there will be increased settling time for power up scenarios when Vbus (or Vcm=Vs) is starting from < 2.7V to final voltage >2.7V. You can reference Figure 7-25 of datasheet for details.

    Sincerely,

    Peter