Part Number: INA200
Hi teams,
I have an issue about amp in INA200.
There is the schematic.VCC is 18V, Vshunt is about 13mV. There is a 47nF cap connected to Amp out.
When the circuit work, output of amp(Pin 2) is a triangular wave, freq is about 50kHz and Vpp is about 700mV.
The freq and Vpp vary with the value of cap(C1).
Then I take off the 47nF cap or change the R1 from 0Ω to 100Ω, this circuit works well.
Some expert say the amp load cap couldn't exceed 10nF.
I want to know the internal mechanism and how to calculate this chip's phase margin.
Thank you so muck.