Part Number: AMC3330
Other Parts Discussed in Thread: AMC3336
Dear expert,
We have a voltage signal of 460KHz, is AMC3330 fit for it's voltage detection?
From Amc3330 datasheet, the output bandwidth is 375KHz, seems this chip couldn't support 460KHz voltage signal detection.
But in the datasheet also mentioned: the internal TRx carrier is 480MHz as below. It's much more higher than 460KHz. Does this 375KHz limitation come from the amplifier stage ( It seems the Isolation stage could support more than 460KHz )?
7.3.2 Isolation Channel Signal Transmission
The AMC3330 uses an on-off keying (OOK) modulation scheme to transmit the modulator output-bitstream
across the capacitive SiO2-based isolation barrier. Fig 7-1 shows the block diagram of an isolation channel. The
transmitter modulates the bitstream at TX IN with an internally generated, 480-MHz carrier and sends a burst
across the isolation barrier to represent a digital one and sends a no signal to represent the digital zero. The
receiver demodulates the signal after advanced signal conditioning and produces the output. The symmetrical
design of each isolation channel improves the common-mode .....
BR&Thanks
Shawn