Part Number: INA849
Other Parts Discussed in Thread: TMUX6222, INA826S, TMUX6122, TMUX7222
Dear Friend
I have a low-power application requiring a power off in standby mode, I use INA849 to measure DC current of a main power line via a shunt resistor. I have a booster to power the INA849 and make sure its Vs+ is always 3V higher than the main power line voltage.
Since the main power line needs to be always powered on even during measurement circuits are in standby mode, I will have to use two resistors connected in series with INA849 inputs to protect the device's input clamping diode and also prevent voltage built-up at Vs+ (through the clamping diode) in standby mode when the Vs+ lost its power.
So the questions become:
1. Is this "resistor in series with inputs of INA849" a good solution to address the issue in my application?
2. What resistance value and what power rating of the protection resistors are good enough to protect the internal clamping diodes if the answer to question one is YES?
3. Is it necessary to prevent voltage build-up at Vs+ when INA849 is powered off? The concern is due to the requirement from the datasheet Vcm MAX = (Vs+) - 2.5V, if we allow voltage build-up at Vs+, Vcm will be (Vs+) - 0.7V. Also, any output of INA849 is not good for other circuits which are powered off. In the worst case, no matter what resistance value of protection resistors, Vcm at inputs of INA849 may be eventually much higher than Vs+, will this damage the device?
Thank you in advance
Tony