Part Number: TLV9061
Other Parts Discussed in Thread: TLV7031, LM393LV, TL331LV, TL391LV
Hello!
I'm using this exact part: TLV9061SQDBVRQ1. I have built the following circuit, with the addition of a 10K pulldown on SHDN.
When I apply a voltage Vin at the non-inverting terminal, the same voltage - a few mV shows up on the V+ pin. If I connect a 100k resistor between 5V & GND, 200uA of current flows. Why is there so much current going into the noninverting terminal through to the V+ pin?
In the context of my circuit, low consumption is critical due to a battery powered application. The opamp is being used as a comparator to shutdown a 5V regulator after the battery has dropped below a certain level. Everything works fine, except for the when the circuit turns off, SHDN goes low, 5V circuit is turned off, Vin from my battery is still making it to to 5V rail, which is enough to turn on several transistors and several hundred uA slips through continuously.