Other Parts Discussed in Thread: INA146
Hello
I am having a problem with the INA146. I get a constant 2-4 VDC out, even with both input terminals shorted together, or with both input terminals shorted to ground. I am running the part on +12VDC single-ended for VCC. The output is set for a gain of 60, and the output amp seems to be working. The input to A2 (pin 8) is around 30-40 mV when the output is abt 2 VDC. When I first turn on the part, the output voltage--always DC--slowly rises from maybe 1.5 or 2 Volts up to about 3.5-4 VDC. It makes no difference what I do with the inputs. I swapped in a couple of new parts and no change. Pin 1, Pin 4 are both grounded. In fact, if I short pis 1-2-3-4 all to ground, I get the same result.
Any ideas on what is wrong?
THe part is marked:
BB INA
146UA
01VN4
Does this imply a date code of 2001? This is a brand new board, our sub must have used some old parts!
Any help or ideas would be much appreciated! Can't seem to get any answers from TI.