Other Parts Discussed in Thread: XTR111, LM1117
Dear Sir,
I am using XTR 111 to convert my 0-3V (PWM based DAC) as 4-20mA. I am powering the XTR111 using a LM1117 ADJ @ 9V/ 1A (12V as I/P). Also I had retained the same circuit as mentioned in your reference design (evaluation board). The MOSFET which I am using is IRFL9014 ( Pchannel, -60V , 1.8A) and the transistor is BC557 (PNP).
The problem:
I am loading the output of DRAIN (with 15E & 10nF), initially with 500E, with a constant Vin (1V). My current flow is constant. As I decrease my resistance further (400E, 300E, 200E, 100E), the current flow remains the same. But as I increase the resistance above 1K, the current flow decreases. I am unable to solve this problem.
What is the logic behind this? How to solve this? What parameters decide the loading limit of XTR111?
Output of the 4-20mA will be fed to a system which will have a load resistance of more than 100K.
Kindly reply me.
With regards,
Jayaraj.A