Other Parts Discussed in Thread: INA168, INA186
Hi All,
I am using the component INA168:
RS = 0.01 OHM
RL = 133KOHM with 100pF parallel capacitor
after it i have buffer amplifier AD8615 with RC output R=10ohm C=1nF and this is connected to ADC
I need to measure current from 0 to 15 amp
when the load current is 1.7A - the RS voltage 17mV
at the output I measured 350mV and the voltage should be 450mV according to data sheet
I don't know why, I didn't sleep all night because of thinking about it.
please help.