Part Number: AMC1300
Other Parts Discussed in Thread: AMC1311,
Dear team,
My customer is evaluating the AMC1300 for voltage sensing and get a problem. Please ignore using AMC1300 for voltage sensing we understood that AMC1311 is better.)
Please refer to the image below.
They are measuring V1 and V2 to find the reason of the system issue. And the result was, V1 = 0.011V and V2 = 0.087V. From them Gain would be V2/V1≒7.91.
It is significantly different than datasheet fixed value (= 8.2±1%_max).
- Could you please give us the expected cause of the issue and help to resolve it?

Best regards,
Yuto