Other Parts Discussed in Thread: TL074, TL074M,
I have had several of these IC burn up.
I am using +24VDC (V+) and -15VDC (V-) so the Vs(V+ - V-) = 39V
The recommended max is 40V and the absolute max is 42V so I know I am at the upper side but I am under the recommendation, so why am I having the IC burn up in equipment at 25 degree C environment ???
I know the TL074M is only rated for a max Vs of 30V but I am not using the M version as from the photo you can clearly see the part number of H after the TL074 of the IC that is not burn.