Part Number: LMV321
Hi
We need to collect 0 to 5 volts from the external input. The test shows that when the input voltage is 0 volts, the voltage at the front end of the op amp is 0 volts, but the voltage at the back end of the op amp is about 0.05 to 0.06 volts, resulting in the voltage collected in the range of 0 to 5 volts is inconsistent with the input voltage.