Other Parts Discussed in Thread: LM339LV, LM2901
Hi Expert,
I have a question about the transition state of LM2901AVQPWR. The following is the circuit diagram of our model, but I found that if 55VCS and CS are connected together and then 3.3V Turn on, I find that the comparator output pin2 (55VCS) and Pin1 (CS ) will have a time difference of 66ms. Please tell me that this IC contains four comparators, but if the input signals are simultaneous in the application, will there be a time difference in the output 
Eddie