Hello!
I am using the TLV9034 and I have a difficulty.
I am using it in the basic mode without hysteresis.The following is a list of characteristics of the schematic:
V+ :3.3V;
V- : 0V(GND);
IN+:input signal,amplitude from 6mV to 50mV random,FWHM is about 200ns with fast rise time and slow fall time;the input resistance=100Ω.
IN-:Threshold=20mV;the input resistance=100Ω.
OUT:50Ω load.
I connect the IN+ and OUT to the oscilloscope with 1MΩ load, and only when the input signal is higher than about 35mV, there can be TTL output.
I wonder whether the phenomenon is normal,if not then how can I solve this problem.
Thank you so much