Part Number: INA828
Other Parts Discussed in Thread: INA326
Hi,
I am trying to simulate in LTspice the next circuit using INA828:
Vptp = 4V
Vcommon = 2.5v
Vref = 2.5V
Gain = 1
Vcc = 5V
Vee = 0V

I expect to receive output signal between 0.5-4.5V (2.5V +- 2V )
according to datasheet it's suppose to work:

this is my result:

what am I missing? why the limits of the output are 1.5-3.5V?
Thank you is advance,
Roman