This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3217EVM: What is the significance of the extra 10kohm or 20kohm resistor between the test point and trace?

Part Number: THS3217EVM
Other Parts Discussed in Thread: THS3215EVM, , THS3217

Hello, engineers:
I would like to ask a question, in the application THS3215EVM and THS3217EVM (SBOU161A), I see a lot of test points are not directly added to the trace, but connected to the trace through 10kohm or 20kohm resistors. What is the significance of doing this?
I found in the test, when testing a 1kHz sine signal with THS3217 amplification, if the signal is not directly measured through the resistor (ordinary single-ended probe directly touching the pads), although you can also see the shape of the sinusoid, but the signal appears to be banded, amplifying the signal to see a lot of oscillation. While the signal is completely normal when tested through the test point. Is this related to the resistance attached to this test point? Or is it a problem related to my layout design?
Looking forward to your reply!