Part Number: AMC1311-Q1
hi expert
taking TCVOS as an example,

There is a comment(1) in datasheet.

do we use one standard deviation (sigma) or six standard deviation (sigma) to describe these parameters?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC1311-Q1
hi expert
taking TCVOS as an example,

There is a comment(1) in datasheet.

do we use one standard deviation (sigma) or six standard deviation (sigma) to describe these parameters?
Hi Jay,
Thank you for your question. Comment (1) is specifying that the TYP value range includes one standard deviation. The TCV_os typical value is a range of +/-3uV/C. This range includes values that are within one standard deviation. I believe the minimum and maximum are just the edge values of the parameter. I do not think the min and max are calculated using a mean and standard deviation if that is what you are asking.
Is there a reason you want to know how this range is defined? Please let me know.
Best regards,
Eva
Hi Jay,
The min and max values specified in the data sheet are tested values. You should never find a device with greater than the maximum TCV_os of 10 or less than the minimum TCV_os of -10. These values are not calculated using the standard deviation.
When you say six standard deviations, do you mean three in each direction? If so, and you are trying to determine whether 99.7% of the data are within the min and max, it is more than this. The min and max specify 100% of the values should fall in this range.
Best regards,
Eva
hi Eva
The min and max values specified in the data sheet are tested values. You should never find a device with greater than the maximum TCV_os of 10 or less than the minimum TCV_os of -10. These values are not calculated using the standard deviation.
ok got it. I am wrong before.
When you say six standard deviations, do you mean three in each direction? If so, and you are trying to determine whether 99.7% of the data are within the min and max, it is more than this. The min and max specify 100% of the values should fall in this range.
i remember it seems like value in datasheet refer ±6sigma (6 sigma in each direction) data. is it right?