Part Number: INA237
Hi,
according to the datasheet the INA237 has a config register in which you can set bit 15 (RST) to 1 in order to trigger a system reset.
Is it possible to set this bit to 1 and send all other bits of the config register in one i2c transaction?
The use case would be be: user wants to change the configuration of the chip and before everything is set to new values all registers a reset to theri defaults.
So which of the following is the right approach:
1. Set Bit 15 to one and send it to the chip. Then send the rest of the configuration (CONFIG, SHUNT_CAL,etc)
2. Set Bit 15 to one and send the rest of the configuration (CONFIG, SHUNT_CAL,etc) with it to the chip
if 1. is the correct usage: How long does it take for the system reset to occur?
Thanks!
Best regards
Steffen